Security - Johnson Controls - LIT-12013739 - Software Application - OpenBlue Enterprise Manager - 4.4

OpenBlue Enterprise Manager Guide Specification

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12013739
Version
4.4
Revision date
2023-05-17

OBEM uses industry-standard system security and encoding protocols to protect against unauthorized access to data and control systems, including the following security features:

  • All OBEM components (UI, API) use HTTPS, HTTP Strict Transport Security and SSL Certificates to prevent unauthorized access to secure encrypted communication.
  • Supported services such as OBEM Gateway, or data collector, uses self-signed certificates installed on supported products with the option of configuring trusted certificates.
  • Users hold various roles with respective, configurable rights, and data is available based on these specific roles.
  • OBEM application prompts users to change their passwords every sixty days.
  • OBEM supports active directory. Users can use their organization credentials to log on to application. There is no need to manage multiple credentials and passwords.