The Healthy Buildings Reports sections provides the following report:
- IAQ Report
-
The Indoor Air Quality (IAQ) report is available in the Healthy Building Report section of the Report application. The report provides users with a view of how the IAQ of a space is being maintained for both the occupied and unoccupied hours. The report breakdowns the IAQ parameters of Temperature, Humidity, CO2, PM2.5, PM10, and VOC, and shows the user how long their scores were categorized as Good, Moderate, Poor, or Hazardous. The report also gives users insights into the possible reasons behind the scores. This helps users to identify the spaces with poor air quality and take the necessary steps to improve it.
The IAQ report also has an exceptions section that analyzes the space’s IAQ score and reports the deviations from the user-defined Good category. This data helps the user to understand the anomalies in the IAQ and can also help the user to identify possible abnormal sensor behavior.