Energy tracker with baseline - Johnson Controls - LIT-12013739 - Software Application - OpenBlue Enterprise Manager - 4.4

OpenBlue Enterprise Manager Guide Specification

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document type
User Guide
Document number
LIT-12013739
Version
4.4
Revision date
2023-05-17

An energy consumption tracker displays at portfolio, location or building level, and shows the energy consumption of all commodities. Users can view the consumption data of commodities in either a chart or tabular format. The tracker shows the consumption of commodities for the current month. A Summary chart is configurable to show data by week, by month, 3 months, 6 months or by year, and can be exported as an SVG, PNG, JPEG image or as a PDF file.

Energy tracker with baseline provides users with a quick method to assess and compare the consumption, demand only for electricity, against the target baseline.

With the tracker, users can define a baseline across commodities, such as electricity, natural gas, hot water, and chilled water, at both space and meter level, and display the difference between that information and consumption in an easy-to-understand graphical representation.