Energy Manager automatically collects, analyzes, and displays information for all configured physical meters, online and offline meters, and virtual meters located in a facilities operation. Users can easily track, analyze, and manage energy use, for thermal, water, electrical storage, and carbon.
Users can view Key Performance Indicators (KPIs) with their preferred unit of measurement or standard KPIs supplied by OBEM. OBEM helps the user compare and forecast energy use across a portfolio for each building, floor, or location, and by equipment or asset.
The information for energy demand and consumption is available for aggregation and display using various out-of-the-box dashboards.
Users can create and configure custom dashboards to their own needs with OBEM’s define your dashboard feature. For example, a user can define a dashboard to compare consumption of multiple locations, buildings, floors, or meters.
The automated reporting tool can generate easy-to-understand summary reports from the dashboard data.
In addition to this, Energy Manager provides the capability to measure the consumption against baseline and notify the user if consumption is approaching or exceeding the baseline.
OBEM supports the following languages:
- English
- German
- Chinese (Simplified)
- Spanish (European)
- Portuguese (Brazilian)
- Italian
- Japanese
- French
- Dutch
- Korean
- Arabic
- Hebrew
The following additional features are detailed in this guide specification:
- Map Selection
- Energy Density Dashboards
- Weather Normalization
- Energy Tracker with Baseline
- Energy Summary of Commodities
- Energy Fault Detection and Diagnostics (FDD)
- Energy Forecast
- Building Benchmarking
- Building EUI Comparison
- Internal Benchmarking
- EUI vs. Consumption
- Define Your Dashboard: Configure dashboards to display data for space or meters.
- Consumption and Demand Comparisons
- Energy Profiling
- Consumption Profiling
- Demand Profiling
- Data Cleansing and Normalization
- User Defined Baseline
- Energy Summary Reports with Auto Scheduling
- Energy Impact Report monetizing faults throughout the platform
For more information, see Energy Manager dashboards.
Use OBEM, on its own or coupled with an Asset Performance software add-on, to provide ease of access to enterprise performance comparisons and life cycle management information to enhance user insight into site operations.