Verify that you have the Johnson Controls extended application and data server (ADX or ADS) system configuration that you require to install OpenBlue Enterprise Manager. Contact your Johnson Controls administrator to obtain the following information:
- Johnson Controls application and data server (ADS or ADX) software version number. EM supports Johnson Controls release 5.2 and higher.
-
Johnson Controls system user credentials. You must
create a dedicated read-only user account in the SQL instance of the Johnson Controls system. EM uses this account to access the trend data. For example,
mem_readonly. - Microsoft SQL ServerĀ® name and IP address.
- Microsoft SQL Server read-only user account. For more information, see Creating a SQL Server read-only user account.
-
Johnson Controls analog trend extension. Use the following table to enable trend
extensions for analog points for both hardware and software data collectors:
Table 1. Trend extensions for analog points Attribute Value Name Trend - Present Value Description Object Type Rend Log Enable True Start Time Unspecified Stop Time Unspecified Buffer Size 144 Stop When Full False Sample Interval 900 seconds Client COV Increment Repository Enabled True Transfer Setpoint 4
Note: The sample interval is set at 900
seconds automatically. If you decide to change this frequency in the OpenBlue Enterprise
Manager application, the meter automatically updates to your selected time frame after its
next 900 second interval. This only applies to the Johnson Controls
Aaeon Box.
-
Johnson Controls binary trend extension. Use the following table to enable trend
extensions for binary points for both hardware and software data collectors:
Table 2. Trend extensions for binary points Attribute Value Name Trend - Present Value Description Object Type Trend Log Enable True Start Time Unspecified Stop Time Unspecified Buffer Size 20 Stop When Full False Sample Interval 0 Client COV Increment 1.0 Repository Enabled True Transfer Setpoint 1
For more information, refer to the OpenBlue Enterprise Manager Implementation Planning Guide (LIT-12012563) and the Metasys SMP Help (LIT-1201793).
- System configuration tool (SCT) archive backup file.
- Microsoft SQL Historian DB archive backup file. For more information, refer to the Metasys Database Manager Instructions (LIT-12011553).