Configuring data collectors - Johnson Controls - LIT-12012431 - Software Application - OpenBlue Enterprise Manager - 4.0

OpenBlue Enterprise Manager Data Collector Installation Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Enterprise Manager
Document number
LIT-12012431
Version
4.0
Revision date
2021-11-29

OpenBlue Enterprise Manager supports Johnson Controls systems and third-party building management systems with the BACnet® IP protocol.

Use this guide to connect your building management system to EM and to discover devices and data points. You can configure both Johnson Controls and BACnet® IP data collectors in the same instance of EM.

Note: For hardware, place the data collector on a stable, flat and dry surface in an environmentally controlled space that has sufficient air circulation, such as a server room.