Trends - Johnson Controls - LIT-12014192 - Chiller management portal - Smart Connected Chillers - v2023.Q2

OpenBlue Connected Chillers Branch Facing Dashboard User Guide

Product
Building Automation Systems > Building Automation Systems > Smart Connected Chillers
Document number
LIT-12014192
Version
v2023.Q2
Revision date
2023-07-13

On the Trends dashboard, you can select to view the UOM in Imperial (IP) or Metric (SI). The default UOM is selected in the To Unit configuration.

You can add limits under the UOM selection, these limits display on the dashboard. If you add limits for the Metric or the Imperial selection of data points, then the limits display accordingly.

For more information, see Navigating to the trends dashboard.