Not in scope - Johnson Controls - LIT-12014192 - Chiller management portal - Smart Connected Chillers - v2023.Q2

OpenBlue Connected Chillers Branch Facing Dashboard User Guide

Product
Building Automation Systems > Building Automation Systems > Smart Connected Chillers
Document number
LIT-12014192
Version
v2023.Q2
Revision date
2023-07-13
The following options are not available for UOM:
  • For IOM (flow meter and energy meter data points) and calculated data points such as cooling efficiency and cooling capacity, the UOM conversion functionality is not applicable. For these data points, the same value, the source received value, displays with the unit type.
  • Automatic data point unit detection and conversion.