Configuring thresholds - Johnson Controls - LIT-12014192 - Chiller management portal - Smart Connected Chillers - v2023.Q2

OpenBlue Connected Chillers Branch Facing Dashboard User Guide

Product
Building Automation Systems > Building Automation Systems > Smart Connected Chillers
Document type
User Guide
Document number
LIT-12014192
Version
v2023.Q2
Revision date
2023-07-13

If you create a pre-condition with the constant template then you need to enter threshold values for that particular created constant template so the pre-condition executes with the configured value.

About this task

To configure a threshold value at asset level, complete the following steps:

Procedure

  1. From the Customer list, select a customer.
  2. From the Facility list, select a facility.
  3. From the Asset list, select a chiller.
  4. From the Constant list, select an existing constant template.
  5. In the Value field, enter the value of the threshold.
  6. In the Tag field, enter a tag.
  7. In Excel Upload, click Choose File to upload an Excel file with the constant template threshold values.
  8. Click Add to add the thresholds