Configuring constant templates - Johnson Controls - LIT-12014192 - Chiller management portal - Smart Connected Chillers - v2023.Q2

OpenBlue Connected Chillers Branch Facing Dashboard User Guide

Product
Building Automation Systems > Building Automation Systems > Smart Connected Chillers
Document number
LIT-12014192
Version
v2023.Q2
Revision date
2023-07-13

About this task

To create a new constant template in the Constant Template tab, complete the following steps:

Procedure

  1. From the Equipment Type list, select a chiller.
  2. From the Constant list, select an existing constant template.
  3. From the Tag list, select a tag. The default tag is custom.
  4. In the Description field, enter a description for the constant template.
    Note: The constant template is available in the Add-Pre-Condition window, click on the Add icon to create a constant template.