Thresholds and constant templates - Johnson Controls - LIT-12014192 - Chiller management portal - Smart Connected Chillers - v2023.Q2

OpenBlue Connected Chillers Branch Facing Dashboard User Guide

Product
Building Automation Systems > Building Automation Systems > Smart Connected Chillers
Document number
LIT-12014192
Version
v2023.Q2
Revision date
2023-07-13

To navigate to the thresholds and constant templates tabs from the home page, click the Menu options icon, select Configure, and select the Constants Configuration tab.

There are two tabs in Constants Configuration
  • Thresholds
  • Constant Template
There are two options to create a constant template:
  • In the Constants Configuration tab
  • In the Custom Notification tab, click Add Pre-Conditions. For more information, see Adding pre-conditions.