Removing a fault - Johnson Controls - LIT-12014192 - Chiller management portal - Smart Connected Chillers - v2023.Q2

OpenBlue Connected Chillers Branch Facing Dashboard User Guide

Product
Building Automation Systems > Building Automation Systems > Smart Connected Chillers
Document number
LIT-12014192
Version
v2023.Q2
Revision date
2023-07-13

Admins can select any fault description and choose to remove it from the notification rules or from the rules of a specific country. The remove fault function is available only for Branch Admins and Super Admins.

About this task

To remove a fault, complete the following steps:

Procedure

  1. In Subscriptions, select the Remove Fault Description tab.
  2. From the Chiller Model list, select a model.
  3. From the Fault Type list, select a fault.
  4. From the Fault Description list, select a description.
  5. From the Applicable On list, select all or a country.
    Note: For notification rules that have only one entry in the fault description, you cannot remove it as the fault description is a mandatory field of notification rule.
    Figure 1. Remove a fault