Notification rules grid has following columns:
| Name | Description |
|---|---|
| ID | A unique 6-digit ID automatically generated by the system for the notification rule. |
| Notification category | Displays the category of the notification, such as panel codes or health check. |
| Chiller model |
Displays the chiller model you select when creating the notification rules. The chiller model is only selected in the case of the panel code and health check notification. In the other cases where the chiller model is not selected, the field displays Not Applicable. |
| Customer |
Displays the customer selected during the notification configuration. Note: Each row shows one customer that is
linked to the facility. If multiple customers are selected
during the notification configuration, then multiple records
create for every facility.
|
| Facility |
The facility name is the name you select during the notification configuration. Note: Each row shows one facility. If multiple
facilities are selected during the notification configuration,
then multiple records are created for the facility.
|
| Chiller | Displays the chillers selected for each facility. |
| Fault type | Displays one or multiple fault type selected during the notification configuration. |
| Fault description | Displays one or multiple fault descriptions selected during notification the configuration. |
| Recipient type | Displays the recipient type selected during notification configuration. For example, branch user or customer. |
| Recipient | Displays the recipient selected during the notification configuration.
Note: If you select multiple recipients
from multiple facilities, the record shows the recipients
associated with the facility.
|
| Edit icon | Opens the rule in edit mode. |