Notification rules grid columns - Johnson Controls - LIT-12014192 - Chiller management portal - Smart Connected Chillers - v2023.Q2

OpenBlue Connected Chillers Branch Facing Dashboard User Guide

Product
Building Automation Systems > Building Automation Systems > Smart Connected Chillers
Document type
User Guide
Document number
LIT-12014192
Version
v2023.Q2
Revision date
2023-07-13
Notification rules grid has following columns:
Table 1. Notification rules grid columns
Name Description
ID A unique 6-digit ID automatically generated by the system for the notification rule.
Notification category Displays the category of the notification, such as panel codes or health check.
Chiller model

Displays the chiller model you select when creating the notification rules.

The chiller model is only selected in the case of the panel code and health check notification.

In the other cases where the chiller model is not selected, the field displays Not Applicable.

Customer

Displays the customer selected during the notification configuration.

Note: Each row shows one customer that is linked to the facility. If multiple customers are selected during the notification configuration, then multiple records create for every facility.
Facility

The facility name is the name you select during the notification configuration.

Note: Each row shows one facility. If multiple facilities are selected during the notification configuration, then multiple records are created for the facility.
Chiller Displays the chillers selected for each facility.
Fault type Displays one or multiple fault type selected during the notification configuration.
Fault description Displays one or multiple fault descriptions selected during notification the configuration.
Recipient type Displays the recipient type selected during notification configuration. For example, branch user or customer.
Recipient Displays the recipient selected during the notification configuration.
Note: If you select multiple recipients from multiple facilities, the record shows the recipients associated with the facility.
Edit icon Opens the rule in edit mode.