Notification categories - Johnson Controls - LIT-12014192 - Chiller management portal - Smart Connected Chillers - v2023.Q2

OpenBlue Connected Chillers Branch Facing Dashboard User Guide

Product
Building Automation Systems > Building Automation Systems > Smart Connected Chillers
Document number
LIT-12014192
Version
v2023.Q2
Revision date
2023-07-13
You can add a notification category when you create a new notification rule. The notification categories are:
To add a notification category, complete the following steps:
  1. From the Menu options icon, select Notifications.
  2. Click Add Notification and select the type of notification you want to create.
  3. Click Next.
You can create notification rules for a single chiller or create a mass notification for multiple chillers.
Note: If you create a mass notification and select chillers from different facilities and customers, then different notification records are created for each facility. Each record is assigned with a unique 6-digit notification ID.
Figure 1. Notification categories

For more information on how to create a notification rule, see Creating a notification rule