Chiller checks - Johnson Controls - LIT-12014192 - Chiller management portal - Smart Connected Chillers - v2023.Q2

OpenBlue Connected Chillers Branch Facing Dashboard User Guide

Product
Building Automation Systems > Building Automation Systems > Smart Connected Chillers
Document number
LIT-12014192
Version
v2023.Q2
Revision date
2023-07-13

The Chiller checks section displays performance checks for the selected chiller from the chiller status table.

Figure 1. Chiller check

The Check Type is set to Performance Check by default, you can also choose Status Check.

The Chiller is the default chiller selected in chiller status table. You can select another chiller of the same facility and view the performance check for that chiller.

The graph displays 10 days of CPI score along with its penalty details for each day.

You can hover over the penalty bar and see the details of the fault. Click the fault bar to generate a diagnostic report or chiller health summary depending on the type of fault.

If the performance data is not available, then the message No active performance check data available for previous 10 days displays.