Configuring the Trends dashboard data charts - Johnson Controls - LIT-12014192 - Chiller management portal - Smart Connected Chillers - v2023.Q2

OpenBlue Connected Chillers Branch Facing Dashboard User Guide

Product
Building Automation Systems > Building Automation Systems > Smart Connected Chillers
Document number
LIT-12014192
Version
v2023.Q2
Revision date
2023-07-13
You can customize the data panes in the following ways:
  • To view a data charts for the entire year, click the Calendar icon.
  • To view the chart as a grid or a line chart, click the View Chart Options icon, and click either the Grid data icon or the Line chart icon.
  • To export the data, click the View Chart Options icon and click the Export to CSV icon or the Export to PDF icon.
  • To add notes or recommendations to the data chart, click the View Chart Options icon and click the Notes and Recommendation icon. Select Add Notes or Add Recommendation. For notes, the type, title, and description fill automatically.

    For more information, see Navigating to the notes dashboard.

  • To maximize the size of the chart or grid, click the Maximize Chart icon.
  • For a multi year comparison, click the Calendar icon to select the year, and select the comparison year from the list.