Raw Data Report - Johnson Controls - LIT-12014192 - Chiller management portal - Smart Connected Chillers - v2023.Q2

OpenBlue Connected Chillers Branch Facing Dashboard User Guide

Product
Building Automation Systems > Building Automation Systems > Smart Connected Chillers
Document number
LIT-12014192
Version
v2023.Q2
Revision date
2023-07-13

A Raw Data Report displays raw data for chillers.

About this task

To generate a Raw Data Report, complete the following steps:

Procedure

  1. Navigate to the Reports dashboard. See Navigating to the reports dashboard.
  2. From the Reports list, select Raw Data Report.
  3. From the Customer list, select a customer.
  4. From the Facility list, select a facility.
  5. From the Asset list, select a chiller.
  6. To select an asset point, click Select Points. Select the points, and click Save.
  7. From the Start Date calendar, select a start date.
  8. From the End Date calendar, select an end date.
  9. For Unit of Measure (UOM), click Imperial (IP) or Metric (SI).
  10. Select one option from the 15 Min, Hourly, or Complete Raw Data check boxes.
  11. Click Generate Report.
    Note: A complete 90-day Raw Data Report for Smart Connect Chillers (SCC) displays the data in six time-referenced datasets of reports. Each report covers 15 days.