About this task
To view and export performance data on a chiller for a selected period of time, complete the following steps:
Procedure
- Navigate to the Performance Index dashboard. See Navigating to the performance index dashboard.
- From the Equipment list, select a chiller.
-
Click the Calendar icon
to select a date and click Show.
Alternatively, select from the available time frame options on the right-side of the screen. You can select from periods of 10 days or one month.
-
To change the time period in the selected parameters, drag the
blue rectangles on the Status bar.
The colors for the time periods are as follows:
- Green: On
- Light gray: Off
- Dark gray: No data available
- To add notes to a performance trend, in the Performance Trend menu, click the Notes icon.
-
To export performance index data or penalty history data, click
the Export to CSV icon in the pane.
Note: For information about how the Performance Index is calculated in Performance Trend Status, click the Information icon.