Adding a note in the facility tab - Johnson Controls - LIT-12014192 - Chiller management portal - Smart Connected Chillers - v2023.Q2

OpenBlue Connected Chillers Branch Facing Dashboard User Guide

Product
Building Automation Systems > Building Automation Systems > Smart Connected Chillers
Document type
User Guide
Document number
LIT-12014192
Version
v2023.Q2
Revision date
2023-07-13

About this task

To add a note in the facility tab, complete the following steps:

Procedure

  1. In the Notes dashboard, click the Facility tab.
  2. Click Add Notes.
  3. In the Add Notes window, from the Type list, select the type of note.
  4. In the Title field, enter a title.
  5. In the Description field, enter a description.
  6. To upload a reference file, click Choose Files.
  7. To add a comment to the note, enter a comment in the Comment field, and click Add.
    Note: You can add more than one comment, and any user with the relevant access can add a comment.
  8. Click Save.