About this task
Procedure
- In the Notes dashboard, click the Chiller tab.
- From the Equipment list, select a chiller.
- Click Add Notes.
- In the Add Notes window, from the Type list, select the type of note.
- In the Title field, enter a title.
- In the Description field, enter a description.
- To upload a reference file, click Choose Files.
-
To add a comment to the note, enter a comment in the
Comment field, and click Add.
Note: You can add more than one comment, and any user with the relevant access can add a comment.
- Click Save.