Navigating to the notes dashboard - Johnson Controls - LIT-12014192 - Chiller management portal - Smart Connected Chillers - v2023.Q2

OpenBlue Connected Chillers Branch Facing Dashboard User Guide

Product
Building Automation Systems > Building Automation Systems > Smart Connected Chillers
Document type
User Guide
Document number
LIT-12014192
Version
v2023.Q2
Revision date
2023-07-13

The Notes dashboard contains all notes and documents added to the application.

To navigate to the Notes dashboard from the home page, click View Chiller next to a chiller in the Chiller Status table or click a chiller from the navigation tree. On the Chiller dashboard, click the Notes tab.

Figure 1. Notes dashboard
The Notes dashboard contains two tabs:
  • Facility: This tab contains notes and documents added to the facilities.
  • Chiller: This tab contains notes and documents added to the chillers.
Both tabs have two sections, the upper section contains notes and the lower section contains documents.
Note: You can also access these notes on the Overview dashboard in the Facility Feeds pane.
You can add Notes from the following locations in the application:
  • Trends dashboard
  • Comparative dashboard
  • Performance index dashboard
  • Notes dashboard
    • Chiller information
    • Facility feeds