Adding a chart - Johnson Controls - LIT-12014192 - Chiller management portal - Smart Connected Chillers - v2023.Q2

OpenBlue Connected Chillers Branch Facing Dashboard User Guide

Product
Building Automation Systems > Building Automation Systems > Smart Connected Chillers
Document number
LIT-12014192
Version
v2023.Q2
Revision date
2023-07-13

Procedure

  1. Navigate to the Comparative dashboard. See Navigating to the comparative dashboard.
  2. Click Add Chart to create a chart. Select the points you want to add.
    Note: You can compare points for multiple chillers in the same facility.
  3. To filter the available points, enter information in the Search bar.
  4. To remove a selected point from the list, click the Delete icon.
  5. Click OK.
  6. To save the chart as a favorite, in the Confirm window, click Yes. Enter a name for the chart, and click OK.
  7. To view the chart without saving it, click No in the confirm window.
    Note: You can add multiple charts to the Comparative dashboard.