Creating a new visit - Johnson Controls - LIT-12013272 - Software Application - Companion - 2.4

OpenBlue Companion User Guide

Brand
Johnson Controls
Product name
Companion
Document type
User Guide
Document number
LIT-12013272
Version
2.4
Revision date
2021-04-30
Language
English

Procedure

  1. From the settings menu, select My Visitors.
  2. Tap the + icon.
  3. To the Visitor's Name field, add the visitor's name.
  4. To the Email Addresss field, add the visitor's email address. This is the address to which Companion sends the visitor's OTP.
  5. Select the location and date of the visit.
  6. Select the start time and end time of the visit, or click All Day if the visit is an all day visit.
  7. Tap Reserve Parking to reserve a parking space for the visitor. If the visitor requires a disabled parking bay, click Handicap Parking. The visitor receives their automatically assigned parking space in the appointment confirmation email.
    Note: If there are no available parking spaces, the appointment confirmation email advises the visitor to contact an administrator to arrange parking.
  8. Tap Register.