Checking in to a workspace - Johnson Controls - LIT-12013272 - Software Application - Companion - 2.4

OpenBlue Companion User Guide

Brand
Johnson Controls
Product name
Companion
Document type
User Guide
Document number
LIT-12013272
Version
2.4
Revision date
2021-04-30
Language
English
If you do not have a workspace reservation, and if you are on the premises, you can check in to an available workspace for immediate use.
Note: If your workplace has conditional access restrictions to comply with social distancing, you might not be able to check in to a workspace without a reservation. For more information, see Conditional access and maximum capacity.
To check in to a workspace using Bluetooth or NFC, complete the following steps:
  1. On the home screen, tap Check-in.
  2. On the check-in screen, tap Tap to Check-in.
  3. Place your phone near the reader.
  4. Select a duration time and tap Check-in.
To check in to a workspace using a QR code, complete the following steps:
  1. On the check-in screen, tap the QR code icon.
  2. Scan the QR code at your workspace.
  3. Select a duration time and tap Check-in.

When you check in to a workspace, your home screen updates appropriately. You receive a notification before your reservation time expires.

Extending check-in time or checking out

To extend your check-in time, or check-out, complete the following steps:
  1. On the home screen, tap your reserved workspace.
  2. To extend your reservation time, tap Extend, adjust the remaining time, and tap Check-in.
  3. To check out, tap Check-out.