Scalable - Johnson Controls - LIT-12013214 - Software Application - OpenBlue Companion - 2.8

OpenBlue Companion Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Companion
Document number
LIT-12013214
Version
2.8
Revision date
2022-10-21

Companion system architecture is scalable for all customers. Components can be added as needed to support the following aims:

  • Offer the mobile application to different occupant user groups such as tenants, technicians, facility managers, building owners, vendors and contractors, visitors, and more.
  • Integrate with third-party BMS to unify operations with Companion.
  • Enable or disable modular features to grow and adapt to the organization.
  • Integrate multiple applications into Companion over time as investments are made.