Facility team value - Johnson Controls - LIT-12013214 - Software Application - OpenBlue Companion - 2.8

OpenBlue Companion Product Bulletin

Product
Building Automation Systems > Building Automation Systems > OpenBlue Companion
Document type
Product Bulletin
Document number
LIT-12013214
Version
2.8
Revision date
2022-10-21

For the facility team, integrations and workflows automate systems based on occupant behavior. For example, you can set spaces to automatically release when they do not detect an occupant. You can also set light fixtures to automatically turn off to conserve energy when no booking is in place. Companion’s smart spaces support the plans of occupants, but also understand what to do when plans change.