Scheduling an individual space reservation - Johnson Controls - LIT-12014054 - Software Application - OpenBlue Companion - 2.7.1

OpenBlue Companion Desktop User Guide

Product
Building Automation Systems > Building Automation Systems > OpenBlue Companion
Document number
LIT-12014054
Version
2.7.1
Revision date
2022-08-29

Procedure

To schedule an individual space reservation, complete the following steps:

  1. Choose from the following options to open the space reservation page:
    • On the dashboard, in the upper right, click or tap Schedule, and select Individual Reservation .
    • In the Features panel, click or tap Calendar, and select Individual Reservation .
  2. From the relevant lists, select a space type, location, and select any necessary resources.
  3. Select a date and time.
  4. To set up a repeat reservation, click or tap Repeat and select the days for the reservation to repeat on.
  5. For parking space reservation, to reserve a disabled parking bay, select Disabled Parking.
  6. Click or tap Search.
    The spaces that meet the selected requirements appear.
  7. Select the space that you want to reserve, then click or tap Reserve .

What to do next

When your reservation is near, you receive a reminder on the Companion app. If you do not check in to the reserved space in time, the system releases the space.