Concurrent users - Johnson Controls - LIT-1901106 - Software Application - OpenBlue Companion - 2.9

OpenBlue Companion Catalog Page

Product
Building Automation Systems > Building Automation Systems > OpenBlue Companion
Document type
Catalog Page
Document number
LIT-1901106
Version
2.9
Revision date
2024-05-15
Product status
Active

For new Companion orders, the number of concurrent users must be determined. The number of concurrent users is a ratio of the total number of users. The industry-standard value of this ratio is 75%. For example, if the total number of users is 500, the subscription price is calculated to include 375 concurrent users.

The minimum number of concurrent users is 100. You can increase the number of the total users in packets of 25. For example, if the customer wants to license Companion for 105 total users, it needs to be rounded up first to 125 users and multiplied by 0.75 to get the number of concurrent users. The number of concurrent users in this case is less than the minimum of 100, so increase the total number of users to 150, and the number of concurrent users in this case is 113.

Quantity in Companion contracts refers to a year of access for a single user.