To assign rights to a role, complete the following steps:
- From the Home page, in the navigation menu, select User Configuration.
- Click the Roles & Rights tab, and click Create New.
- On the Role Creation screen, in the Role name field, enter a name.
- From the Role type list, select a type.
- On the right side of the screen, click Expand All, and select the appropriate features. Select View Only for view only access, and select Full Control for full control of the feature. Selecting less than all subsections of a feature gives partial control of that feature.
- On the left side of the screen, select the appropriate locations to assign to this role.
- Click Save.