Point mapping - Johnson Controls - LIT-12013271 - Software Application - Companion Workplace Experience Application - 2.8

OpenBlue Companion Admin Portal Configuration Guide

Product
Document number
LIT-12013271
Version
2.8
Revision date
2022-10-21

Map points to a space to associate comfort controls to an area in the building. A user who checks in to the area can view or control the points, for example, change a temperature set point. To configure point mapping, perform the following steps:

  1. Open the Space Configuration tab.
  2. Select the area you want to configure from the Space Tree.
  3. In the Point Mapping section, select a point from the Point mapping list. The point type fills automatically.
  4. Optional: Select a category from the Category list.
  5. By default, the point display name matches the point name. To set a custom name, select the field and type a new name. Press Enter on your keyboard when complete.
  6. Click Save to save your settings.
  7. To remove a point, click Remove beside the point on the list.

    Note: To prevent a workstation from having access to temperature controls, clear the Show temperature set point control check box.