Creating a zone - Johnson Controls - LIT-12013271 - Software Application - Companion Workplace Experience Application - 2.8

OpenBlue Companion Admin Portal Configuration Guide

Product
Document number
LIT-12013271
Version
2.8
Revision date
2022-10-21

About this task

A zone is a section of a floor. Create zones in the Space Tree using the Admin Portal. To create a zone space in the Space Tree, complete the following steps:

Procedure

  1. From the Home page, in the navigation menu, select Space Configuration.
  2. From the Space Tree pane, select the building and the floor where you want to create a zone in.
  3. Click Zone.
  4. Click Add New.
  5. In the Zone name section, enter the name of the zone in all applicable languages.
  6. In the Zone area field, enter the area of the zone.
  7. Click Save.