Creating a common area - Johnson Controls - LIT-12013271 - Software Application - Companion Workplace Experience Application - 2.8

OpenBlue Companion Admin Portal Configuration Guide

Product
Document number
LIT-12013271
Version
2.8
Revision date
2022-10-21

A common area is a section of a floor that numerous employees or building tenants use.

About this task

To create a common area space in the Space Tree, complete the following steps:

Procedure

  1. From the Home page, in the navigation menu, select your location, building, floor, and zone, then select Space Configuration.
  2. From the Space Tree pane, select Common Area.
  3. Click Add New.
  4. From the Location name list, select the location of the common area.
  5. From the Building name list, select the building of the common area.
  6. From the Floor name list, select the floor of the common area.
  7. From the Zone name list, select the zone of the common area.
  8. From the Common area type list, select the type of common area.
  9. In the Common area name field, enter the name of the common area in all applicable languages.
  10. In the Common area description field, enter a description of the common area.
  11. Click Save.