Creating a Skyway - Johnson Controls - LIT-12013271 - Software Application - Companion Workplace Experience Application - 2.8

OpenBlue Companion Admin Portal Configuration Guide

Product
Document number
LIT-12013271
Version
2.8
Revision date
2022-10-21

A Skyway is an enclosed bridge between two buildings.

About this task

To create a Skyway space in the Space Tree, complete the following steps:

Procedure

  1. From the Home page, in the navigation menu, select Space Configuration.
  2. From the Space Tree pane, select Skyway.
  3. Click Add New.
  4. In the Skyway name field, enter the name of the Skyway in all applicable languages.
  5. Click Save.