Configuring navigation routes - Johnson Controls - LIT-12013271 - Software Application - Companion - 2.8

OpenBlue Companion Admin Portal Configuration Guide

Brand
Johnson Controls
Product name
Companion
Document type
User Guide
Document number
LIT-12013271
Version
2.8
Revision date
2022-10-21
Language
English

Procedure

To configure navigation routes, perform the following steps:

  1. From the Home page, in the navigation menu, select Navigation Routes.
  2. Click the Routes tab.
  3. Choose from the following options:
    • To create a new navigation route, click Create New and continue with the next step.
    • To edit a navigation route, click the route's row in the list and continue with the next step.
    • To delete a navigation route, click the Delete icon in the Action column for the route in the list.
  4. In the Route Details page, in the space tree on the left, select the spaces that the route applies to.
  5. Select the language.
  6. For a new route, select the route type and route name.
  7. Enter the display name for the route.
  8. To make the route the default route, select Mark as default.
  9. Click Save.