Creating a QR code for a space - Johnson Controls - LIT-12013271 - Software Application - Companion Workplace Experience Application - 2.8

OpenBlue Companion Admin Portal Configuration Guide

Product
Document number
LIT-12013271
Version
2.8
Revision date
2022-10-21

Use the QR code to place in the corresponding space for users to scan for the Navigation and SOS features. To create a QR code for a space, complete the following steps:

Procedure

  1. From the Home page, in the navigation menu, select Global Configuration.
  2. Click the QR Codes tab, and from the Space List, select a location check box.
  3. Click Generate QR Code. The QR code pop up appears.
  4. Select a location, building, floor, and zone as applicable.
  5. Optional: To use a logo in your QR code, check the Branded QR code check box.
    Note: A logo must have already been uploaded for the portfolio under Space Configuration for this option to be available.
  6. Click Download QR PDF.

Results

The QR code downloads to your device in a PDF format.