Editing a point - Johnson Controls - LIT-12013271 - Software Application - Companion Workplace Experience Application - 2.8

OpenBlue Companion Admin Portal Configuration Guide

Product
Document number
LIT-12013271
Version
2.8
Revision date
2022-10-21

Procedure

To edit a point, perform the following steps:

  1. From the Home page, in the navigation menu, select Comfort Configuration.
  2. On the comfort configuration page, click the Point Configuration tab.
    The list of points with the point name, object ID, object type, and FQR ID is pulled from OpenBlue Bridge automatically.
  3. To edit a point, click the point's row in the list.
  4. Select the point type from the Point type list. If applicable, select a subpoint type from the Sub Point Type list.
  5. To subscribe to a point, from the Subscribe list, select Yes.
  6. If applicable, select a point from the Remote Adjustment Point list.
  7. Click Save.