Procedure
To configure comfort rules, perform the following steps:
- From the Home page, in the navigation menu, select Comfort Configuration.
- On the comfort configuration page, click the Comfort Rules tab.
-
Choose from the following options:
- To create a new comfort rule, click Create New and continue with the next step.
- To edit a comfort rule, click the comfort rule's row in the list and continue with the next step.
- To delete a comfort rule, click the Delete icon in the Action column for the comfort rule in the list.
- For a new comfort rule, select a location, building, and floor. When you edit a comfort rule, you cannot change the location, building, or floor.
- To enable comfort controls for a location, select For location. To enable comfort controls only on space booking, check the For space booking check box.
- To change the temperature unit, use the Set Point Temperature Unit toggle switch.
- To enable or disable temperature control, use the Enable Temperature Control toggle switch.
- Enter a minimum and maximum value in the Set Point Temperature Range fields.
- Select a value from the Temperature Increment in Degrees list.
- In the Default Space Settings section, select the default values for lighting, brightness, temperature, blinds, shades, and other comfort controls.
- Click Save or Update.