Editing cafeteria details - Johnson Controls - LIT-12013271 - Software Application - Companion Workplace Experience Application - 2.8

OpenBlue Companion Admin Portal Configuration Guide

Product
Document type
User Guide
Document number
LIT-12013271
Version
2.8
Revision date
2022-10-21

Procedure

To edit cafeteria language, status, timings, and staff, perform the following steps:

  1. From the Home page, in the navigation menu, select Cafeteria.
  2. On the cafeteria page, click the Cafeteria Configuration tab.
  3. To change whether the cafeteria is open or closed, use the toggle switch in the Cafeteria Status column.
  4. To edit the language, timings and concierge availability, click a cafeteria's row.
  5. Select a language from the list.
  6. If the cafeteria is staffed, select the Concierge available check box.
  7. To edit an existing start and end time, type the time or click the Clock icon to set the time.
  8. To add a new timing, click Add New Timing, and enter the start and end times.
  9. Click Save.