Configuring cafeteria menus - Johnson Controls - LIT-12013271 - Software Application - Companion Workplace Experience Application - 2.8

OpenBlue Companion Admin Portal Configuration Guide

Product
Document type
User Guide
Document number
LIT-12013271
Version
2.8
Revision date
2022-10-21

Procedure

To add or edit cafeteria menu items, perform the following steps:

  1. From the Home page, in the navigation menu, select Cafeteria.
  2. On the cafeteria page, click the Menu Configuration tab.
  3. From the Item List for list, select the cafeteria.
  4. To make an item active or inactive, use the toggle switch in the Item Status column.
  5. To create a new menu item, click Add New. To edit a menu item, click the menu item's row in the list.
  6. In the Item Details page, select a language.
  7. Enter the name of the item, and an optional description.
  8. To make the item available on the kiosk, select Available on Kiosk.
  9. In the Item Tags select if the item is vegetarian, select any allergens that it contains, and select a food preference.
  10. To upload an image for the menu item, click Browse.
  11. Click Save.