Cafeteria - Johnson Controls - LIT-12013271 - Software Application - Companion Workplace Experience Application - 2.8

OpenBlue Companion Admin Portal Configuration Guide

Product
Document number
LIT-12013271
Version
2.8
Revision date
2022-10-21

Create or modify menus for cafeteria locations and modify concierge availability and cafeteria status and timings. An admin or superadmin user can set up a separate role for these cafeteria management tasks, and another role for order management in the cafeteria order fulfillment kiosk. Then the admin or superadmin user can assign the new roles to the relevant users. For instructions that relate to roles, rights, and users, see User configuration. For more information about cafeteria order management, refer to the OpenBlue Companion Cafeteria Order Fulfillment Kiosk User Guide (LIT-12014062).

A cafeteria is a type of common area. To create a cafeteria, create a common area in the space tree and set the space type to Cafeteria / Lunch Area. To create a common area, see Creating a common area.

Figure 1. Cafeteria configuration