Configuring work order fields - Johnson Controls - LIT-12013271 - Software Application - Companion Workplace Experience Application - 2.8

OpenBlue Companion Admin Portal Configuration Guide

Product
Document number
LIT-12013271
Version
2.8
Revision date
2022-10-21

Procedure

To configure work order fields, complete the following steps:

  1. From the navigation panel, select CMMS Configuration.
  2. On the CMMS configuration page, click the Field Configuration tab.
  3. To edit a field configuration, click on a row in the field configuration list.
  4. Select or clear the check boxes for the work order fields.
  5. Click Save.