Configuring CMMS subscriptions - Johnson Controls - LIT-12013271 - Software Application - Companion Workplace Experience Application - 2.8

OpenBlue Companion Admin Portal Configuration Guide

Product
Document number
LIT-12013271
Version
2.8
Revision date
2022-10-21

Procedure

To configure CMMS subscriptions, complete the following steps:

  1. From the navigation panel, select CMMS Configuration.
  2. On the CMMS configuration page, click the Subscribe CMMS tab.
  3. To subscribe to a CMMS, click Create New and complete the following steps:
    1. From the Select CMMS list, select a CMMS to subscribe to.
    2. From the Location list, select the location where the CMMS is used.
    3. From the Buildings list, select one or more buildings where the CMMS is used.
    4. Click Save.
  4. To edit the buildings in a subscription, click the subscription's row in the list, then from the Buildings list, select or clear buildings, and click Save.
  5. To delete a subscription, click the Delete icon in the Action column for the subscription in the list.