Configuring maximum capacity - Johnson Controls - LIT-12013271 - Software Application - Companion Workplace Experience Application - 2.8

OpenBlue Companion Admin Portal Configuration Guide

Product
Document number
LIT-12013271
Version
2.8
Revision date
2022-10-21

Administrators configure the maximum capacity number for a particular date range at specific location and building levels. Users trying to check-in or reserve any space will be compared with available capacity and then allowed to visit the facility and get access to the building. In case the capacity is full, user will not be able to reserve or book spaces.

About this task

To configure maximum capacity restrictions, complete the following steps:

Procedure

  1. From the Home page, in the navigation menu, select Business Rules.
  2. In the top right of the screen, click Create New.
  3. Enter a start date for the restrictions.
  4. Enter an end date for the restrictions.
  5. To the Maximum Capacity field, add the highest number of users to allow into the building. This field only accepts digits.