About this task
Procedure
- From the Home page, select Access Control Configuration. If you have terminal configuration enabled the tab opens automatically.
- Select the terminal type.
- Select the Location.
- If you are configuring a Building Terminal, select the Building.
- If you are configuring a Floor terminal, select the Floor.
- Select the System Type.
- Select the System Name. All terminals matching the selected settings sync from your access control system.
- Click Add Mapping to map the terminal ID with terminal direction and spaces. Once saved, the list of mapped terminals display in the grid.
- To remove the terminal mapping for selected records, click Unmap.