Wiring procedure - Johnson Controls - LIT-12012230 - Nurses Station Display - NSD1380 Nurses Station Display

NSD1380 Nurses Station Display Technical Bulletin

Product
Accessories > Nurses Station > NSD1380 Nurses Station Display
Document type
Technical Bulletin
Document number
LIT-12012230
Revision date
2021-03-29

Procedure

  1. Remove the connectors from the back of the NSD.
  2. See Figure 1 for proper wiring installation. If additional options need to be wired, refer to building prints for a proper wiring diagram.
  3. Plug the connectors back into the NSD.
  4. Carefully push the wires into the electrical box and mount the NSD. Install four screws to hold the pressure monitor firmly to the base.
  5. Press the cover plate onto the NSD1380 Nurses Station Display.
    Figure 1. Modbus communications wiring between RPM1600 Series Room Pressure Monitors,RPC1611 Room Pressure Controllers, and NSD1380 Nurses Station Display

    Important: Wire the NSD exactly as the wiring diagram shows. Making modifications to the wiring may severely damage the unit.
    Important: Use end-of-line (EOL) terminations if the installed device is the last device in the communications chain. The 100 Ohm reference resistors are optional.

Results

If you need assistance installing the system, call Johnson Controls customer service at 1-800-275-5676.