The NSD1380 displays are versatile devices that you can configure to meet your specific application requirements. This section lists all of the menu items, some of which are available to program and change. You can change items by using the touch screen. If you are unfamiliar with the keystroke procedure, please see Configuration for a detailed explanation. This section provides the following information:
- a complete list of all menu items
- the menu item or software name
- each menu item’s function
- the range of values
- the default item value
| Menu item | Software name | Menu item description | Item range | Default value |
|---|---|---|---|---|
| Rescan for connected RPM1600 Series Monitors and RPC1611 Controllers | Rescan | Rescan causes the NSD1380 Nurses Station Display to scan its network to look for connected RPM1600 Series Monitors and RPC1611 Controllers. | N/A | N/A |
| Change Room Modes of Connected RPM1600 Series Monitors and RPC1611 Controllers |
Room Mode |
Room mode selects if the NSD1380 Nurses Station Display can change the room mode of connected RPM1600 Series Monitors and RPC1611 Controllers from the current room mode to NO ISOLATION mode. Note: The NSD1380 Nurses Station Display cannot
change a connected monitor or controller
|
On, Off | On |
| Enable access codes | Passcode |
Passcode prevents unauthorized
access to a menu. If the Passcode item is:
ALL - a Passcode is required to enter the room mode and menu screens. |
Off, Room Mode, Menus, All | Menus |
| Reset settings | Reset Settings |
Reset settings changes all settings to the factory default. Reset settings does not affect calibration. |
N/A | N/A |
| Enable sound | Audible alm | Audible alm enables the audible alarm on the NSD. | On, Off | Off |
| Recalibrate touchscreen |
Touch Cal |
Touch cal starts the touch screen recalibration process. While recalibrating the touch screen, the NSD directs the user to touch the screen in various places. Note: Recalibrating the touch screen is best
accomplished using a stylus, pen, or similar
object.
|
N/A | N/A |