Procedure
-
Tap the button for the room on the touch screen.
Figure 1. Main running screen
-
The Passcode screen appears. To change the room mode, enter passcode
0317 and press Enter.
Figure 2. Passcode screen
-
Tap the preferred room mode at the bottom of the screen.
Figure 3. Room mode selection screen
Note: If you do not select a room mode, the monitor returns to the main running screen after a short delay.Note: The NSD1380 Nurses Station Display cannot change a connected monitor or controller- from NEGATIVE to POSITIVE mode
- from POSITIVE to NEGATIVE mode