LCD touch screen - Johnson Controls - LIT-12012230 - Nurses Station Display - NSD1380 Nurses Station Display

NSD1380 Nurses Station Display Technical Bulletin

Product
Accessories > Nurses Station > NSD1380 Nurses Station Display
Document type
Technical Bulletin
Document number
LIT-12012230
Revision date
2021-03-29

The LCD touch screen displays critical information, including alarm status and room mode.

Table 1. Room icon condition colors
Color Definition
Green The room icon is colored green (NORMAL) when the room pressure and/or other configured measurements are adequate. This light indicates that the room is operating safely. If a setpoint cannot be maintained or an alarm limit has been reached, the icon changes from green to red.
Red The room icon is colored red (ALARM) when the room pressure or other configured measurements exceed alarm limits. This light indicates the room is not operating safely. The LCD screen also indicates the type of alarm or an emergency message.
Gray 1 The room icon is colored gray to indicate No Isolation mode. In No Isolation mode, the device does not alarm.

This operator key can appear on the LCD touch screen:

Table 2. Operator key
Key graphic Key name Key function
MUTE The MUTE key silences an audible alarm. The alarm remains silent until the MUTE TIME value has been reached or the measurement returns to the control setpoint.
1 Due to the blue screen, gray icons appear blue in digital images.