Operator panel - Johnson Controls - LIT-12012230 - Nurses Station Display - NSD1380 Nurses Station Display

NSD1380 Nurses Station Display Technical Bulletin

Product
Accessories > Nurses Station > NSD1380 Nurses Station Display
Document number
LIT-12012230
Revision date
2021-03-29

The NSD1380 Nurses Station Display is easy to use. Room conditions (normal, alarm, no isolation) and room modes (Positive, Negative) appear on the LCD touch screen for up to eight rooms. See the following pages for specific details about the LCD touch screen and controls.

Figure 1 identifies the important features on the LCD touch screen:

Figure 1. Room indicators